test_cookieUsed to check if the user's browser supports cookies.
最大保存期間: 1 日種類: HTTP クッキー
rc::aThis cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
最大保存期間: 永続種類: HTML ローカルストレージ
rc::cThis cookie is used to distinguish between humans and bots.
__cf_bm [x3]This cookie is used to distinguish between humans and bots. This is beneficial for the website, in order to make valid reports on the use of their website.
AWSALB [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
最大保存期間: 7 日種類: HTTP クッキー
AWSALBCORS [x2]Registers which server-cluster is serving the visitor. This is used in context with load balancing, in order to optimize user experience.
conv_variationsThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大保存期間: 永続種類: HTML ローカルストレージ
_conv_rThis cookie is used as a referral-cookie that stores the visitor’s profile – the cookie is overwritten when the visitor re-enters the website and new information on the visitor is collected and stored.
最大保存期間: セッション種類: HTTP クッキー
_conv_sThis cookie contains an ID string on the current session. This contains non-personal information on what subpages the visitor enters – this information is used to optimize the visitor's experience.
最大保存期間: 1 日種類: HTTP クッキー
_conv_vThis cookie is used to identify the frequency of visits and how long the visitor is on the website. The cookie is also used to determine how many and which subpages the visitor visits on a website – this information can be used by the website to optimize the domain and its subpages.
conv_randThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
最大保存期間: 永続種類: HTML ローカルストレージ
_conv_sptestThis cookie is used by the website’s operator in context with multi-variate testing. This is a tool used to combine or change content on the website. This allows the website to find the best variation/edition of the site.
_gaUsed to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大保存期間: 25 ヶ月種類: HTTP クッキー
_ga_#Used to send data to Google Analytics about the visitor's device and behavior. Tracks the visitor across devices and marketing channels.
最大保存期間: 25 ヶ月種類: HTTP クッキー
_gcl_auUsed by Google AdSense for experimenting with advertisement efficiency across websites using their services.
最大保存期間: 3 ヶ月種類: HTTP クッキー
NID保留中
最大保存期間: 6 ヶ月種類: HTTP クッキー
pagead/1p-user-list/#Tracks if the user has shown interest in specific products or events across multiple websites and detects how the user navigates between sites. This is used for measurement of advertisement efforts and facilitates payment of referral-fees between websites.
Beamsplitters are optical components that split light into two directions, and are available in many different designs. Are you interested in learning about the benefits and differences of the multiple types of beamsplitters offered by Edmund Optics, including plate, cube, pellicle, and polka-dot beamsplitters? Join Katie Schwertz, Design Engineer, as she explains the advantages and disadvantages of these beamsplitters. To learn more, read our What are Beamsplitters? application note.
Hi, I’m Katie, one of the Opto-Mechanical engineers here at Edmund Optics. Today I’m going to talk about the different types of beamsplitters we offer and provide you with information that will help you choose what beamsplitter would work best for your application. Beamsplitters are optical components that split light in two directions. For example, they are typically used in interferometers in order for a single beam to interfere with itself. In this setup, you can see laser light passing through a cube beam splitter. Some of the light continues in the direction of the laser, and some of the light is reflected at 90 degrees. We offer several different types of beamsplitters: plate, cube, pellicle and polka dot beamsplitters. A plate beamsplitter is a common type of beamsplitter that is composed of a thin glass substrate with an optical coating optimized for a 45-degree angle of incidence. Advantages of a plate beamsplitter include less chromatic aberration, less absorption due to less glass, and smaller and lighter design compared to a cube beamsplitter. Disadvantages of the plate beamsplitter are the ghost images produced by having light reflect off both surfaces of the glass, lateral displacement of the beam due to thickness of the glass, difficulty to mount without deformation, and their sensitivity to polarized light, which I will discuss later. Cube beamsplitters are essentially composed of two right angle prisms cemented together at the hypotenuse with a partially reflective coating in between. Advantages of the cube include easy mounting, durability of the optical coating since it is between the surfaces, and no ghost images, since reflections propagate back in the direction of the source. Disadvantages of the cube are that it is bulkier and heavier than other types of beamsplitters and doesn’t cover as wide a wavelength range as pellicle or polka dot beamsplitters, though we do offer many different coating options. Also, cube beamsplitters should only be used with collimated beams, since converging and diverging beams contribute to considerable image quality degradation. Pellicle beamsplitters are very thin optical grade film stretched over an aluminum ring and bound in place. They are useful because they have a broad wavelength range of operation, and therefore no chromatic aberration. They have no ghost image, because the front and back surfaces have negligible thickness. They are very lightweight and take up little space in optical systems. The disadvantages of a pellicle beamsplitter are that they are very delicate and easily punctured. Touching the surface will likely ruin the beamsplitter, and great care must be taken when mounting a pellicle to reduce stress and vibration, as these can adversely affect performance. Pellicles are most useful for interferometric applications but can prove to be too costly and delicate for common applications. Polka dot beamsplitters do not split light as typical beamsplitters. Rather, they have a polka dot surface, in which the ‘dots’ are reflective material that cover half the surface, with the other half being transparent. This splits the light much like a conventional beamsplitter does, but has a completely reflective patterned coating, rather than a partially reflective continuous coating as seen in conventional beamsplitters. Advantages of polka dot beamsplitters are that they have a broad wavelength range and their performance is not angle dependent. A disadvantage of polka dot beamsplitters is their lower efficiency, usually around 85%, meaning that about 15% of the light is lost through the system. You may notice that some of our beamsplitters are labeled as ‘polarizing’ or ‘non-polarizing’. Polarizing beamsplitters will reflect S-polarized light and transmit P-polarized light. With non-polarizing beamsplitters, given randomly polarized input light, there will still be some polarization effects, but they depend on the specific type of beamsplitter. For the Edmund Optics TechSpec non-polarizing cube beamsplitters, for example, the difference in reflection and transmission for S and P-pol is less than 6%. If polarization states are not critical for your application, we recommend using non-polarizing beamsplitters I hope this answers your questions about different types of beamsplitters we offer, and which suit your needs. You can browse more of our technical application notes and videos to learn more key concepts and find answers to common questions on our website.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
もしくは 現地オフィス一覧をご覧ください
クイック見積りツール
商品コードを入力して開始しましょう
Copyright 2023, エドモンド・オプティクス・ジャパン株式会社
[東京オフィス] 〒113-0021 東京都文京区本駒込2-29-24 パシフィックスクエア千石 4F
[秋田工場] 〒012-0801 秋田県湯沢市岩崎字壇ノ上3番地