製品がカートに追加されました

Jitter

An imaging phenomenon that limits the accuracy of measurement to at least two pixel separations because signals impinging on the sensor may fall on a pixel or on the space between pixels. Statistically speaking, the latter case may cause a response in the pixel to the immediate left or the immediate right of the space. Due to the standard scan frequency of 60Hz, such a static image will exhibit jitter between the two pixels in question over time. 

See also Pixel

このコンテンツはお役に立ちましたか?
 
販売や技術サポート
 
もしくは 現地オフィス一覧をご覧ください
簡単便利な
クイック見積りツール
商品コードを入力して開始しましょう
This site is protected by VikingCloud's Trusted Commerce program