製品がカートに追加されました

What is the maximum amount of light a polarizer can transmit?

A single perfect polarizer will block 50% of incident light. Add in Fresnel reflections and you are at 42% transmission. For example, our TECHSPEC® Linear Polarizing Laminated Film transmits 38% for a single pass; so only about 4% is being lost to absorption. This is typical for linear polarizers because they are absorptive polarizers. Reflective, or refractive, polarizers like Glan-Thompson will have slightly better transmission, but these are typically not larger than 1” in size thereby limited the applications in which they can be employed.

このコンテンツはお役に立ちましたか?
 
販売や技術サポート
 
もしくは 現地オフィス一覧をご覧ください
簡単便利な
クイック見積りツール
商品コードを入力して開始しましょう