What is the difference between multiple and zero-order retarders and when should I pick one over the other?
Multiple-order retarders (or waveplates) and zero-order retarders are interchangeable. Zero-order waveplates should be considered for more critical applications. The advantages of a zero-order waveplate include an increased bandwidth and a lower sensitivity to temperature changes. A ±2% change from the design wavelength will cause only a minor change in the retardation of a zero-order waveplate. With a multiple-order waveplate, a ±1% change from the designed wavelength will cause considerable problems with the retardation.
このコンテンツはお役に立ちましたか?
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.