当社ではこの種類のCookieは使用していません。
Imaging lenses feature a wide variety of lens mounts, all of which offer different benefits. For a more comprehensive breakdown of these types and what they are useful for, read Lens Mounts. The most common mounts used in machine vision are the C-Mount, S-Mount (M12 mount), F-Mount, TFL-Mount, and TFL II Mount. The C-Mount, S-Mount, TFL-Mount, and TFL II Mount types offer robust stability for machine vision systems whereas the bayonet-style mount of the F-Mount lends itself better to non-industrial, photography-type applications. However, the most useful mount type depends on the size of the machine vision camera sensor being used as well as the optical abilities of the imaging lens.
もしくは 現地オフィス一覧をご覧ください
クイック見積りツール
商品コードを入力して開始しましょう
Copyright 2023, エドモンド・オプティクス・ジャパン株式会社
[東京オフィス] 〒113-0021 東京都文京区本駒込2-29-24 パシフィックスクエア千石 4F
[秋田工場] 〒012-0801 秋田県湯沢市岩崎字壇ノ上3番地